Hello,
We use the AM654x IDK Board with processor_sdk_rtos_am65xx_5_03_00_07. In our user case, we only need one ARM Cortex R5F core. To save power we have to disable the other unused cores of the processor.
When we load the sysfw.bin File in the SBL during bootup all cores and modules get powered up. We tried to shutdown modules with Sciclient_pmSetModuleState(..) in the SBL File and with PMLIBSysConfigSetPowerState(..) in a C – Program, but if we read back the current state, all modules are still powered on.
Is it possible to deactivate the unused cores with a function in the SBL code, or should the sysfw.bin be reconfigured?
Is the source code of the SYS Firmware available?
Best Regards
Marco