Tool/software: TI C/C++ Compiler
Hi,
With Jacinto6 baord and after ROM download the u-boot-spl.bin From Ubuntu Host.
sudo ../emmc_files/usbboot-stand-alone -S spl/u-boot-spl.bin
reading ASIC ID
CHIP: 5641
rom minor version: 02
IDEN: 0000000000000000000000000000000000000000
MPKH: 0000000000000000000000000000000000000000000000000000000000000000
CRC0: 51d2f9a7
CRC1: 00000000
device is GP
sending 2ndstage to target...
On Target console, there is no output.
Welcome to minicom 2.7
OPTIONS: I18n
Compiled on Nov 15 2018, 20:18:47.
Port /dev/ttyUSB0, 17:51:40
Press CTRL-A Z for help on special keys
and the board fails to boot
SYSBOOT[ 0-15] => 0000 0000 1000 0001 // I tried also with EMMC, SINGLE BOOT SPL and SD
SW5: 00101 11000
Any idea about this issue ?
Thanks,
Chokri