Other Parts Discussed in Thread: TIDA-00299
Hi,
a customer is connecting 2x DP83822 PHYs on the 2x PRU MII interfaces and wants to configure two things on bootup
[] Put the AM3352 into 25MHz crystal mode via SYSBOOT[15:14] = 10b, here the SYSBOOT[15]=1 and is also pr1_mii0_rxdv, a pin connected to the DP83822 RXDV.
[] Put the DP83822 into MII mode with 25MHz reference clock. This would require RXDV to be low, however.
So there is a miss-match, which is also present in the TIDA-00299.
That reference design pulls RXDV high, therefore starting the DP83822 in RMII mode, instead of MII mode, which is required by the PRU.
Is it ok to start the DP83822 in RMII mode and then write to the RMII register RCSR and put it into MII mode and 25MHz mode after the AM3352 bootup?
Regards,
--Gunter