Other Parts Discussed in Thread: HVDA551-Q1
What is the default output voltage level of DCAN in TDA3x RVP.
Is it 1.8V or 3.3V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the default output voltage level of DCAN in TDA3x RVP.
Is it 1.8V or 3.3V?
Hi Akshatha,
The voltage level of DCAN pins in TDA3x RVP is 3.3V.
Thanks & Regards,
Vivek Dhande.
Texas Instruments (India) Pvt Ltd
Hi Vivek,
I came across the datasheet for TDA3x. The CAN transceiver being used here is HVDA551-Q1, which supports both 3.3V and 5V. We are trying to interface TDA3X to another board for CAN communication. For this, there is a need to convert the DCAN voltage level to 5V. How will I be able to do this?
Thanks
Hi Akshatha,
Typically, there is a range for these I/O voltages. 3.3 V should come in this range for this device.
Thanks & Regards,
Vivek Dhande.
Texas Instruments (India) Pvt