Other Parts Discussed in Thread: TEST, GRACE, LM90, LM95245, TMP102, TFP410, CYPRESS, TPS65217, TPS65218, TPS65910, TWL6040, TPS65090
Hi,
I am doing a Yocto Build for my AM4378 Based Board.
I am following steps mentioned on software-dl.ti.com/.../Overview_Building_the_SDK.html
While doing bitbake of complere SDK, I am getting following error logs:
ravi@dgnu-sgnt-kvm02:~/Yocto_Build/tisdk/build$ MACHINE=am437x-evm bitbake arago-core-tisdk-bundle
WARNING: Layer meta-processor-sdk should set LAYERSERIES_COMPAT_meta-processor-sdk in its conf/layer.conf file to list the core layer names it is compatible with.
WARNING: Layer browser-layer should set LAYERSERIES_COMPAT_browser-layer in its conf/layer.conf file to list the core layer names it is compatible with.
WARNING: Layer meta-processor-sdk should set LAYERSERIES_COMPAT_meta-processor-sdk in its conf/layer.conf file to list the core layer names it is compatible with.
WARNING: Layer browser-layer should set LAYERSERIES_COMPAT_browser-layer in its conf/layer.conf file to list the core layer names it is compatible with.
Loading cache: 100% |############################################################################################################| Time: 0:00:03
Loaded 4730 entries from dependency cache.
WARNING: No recipes available for:
/home/ravi/Yocto_Build/tisdk/sources/meta-processor-sdk/recipes-ros/navigation/move-base_1.12.14.bbappend
/home/ravi/Yocto_Build/tisdk/sources/meta-processor-sdk/recipes-ros/navigation/rotate-recovery_1.12.14.bbappend
NOTE: Resolving any missing task queue dependencies
NOTE: Multiple providers are available for runtime python-bson (python-bson, python-pymongo)
Consider defining a PREFERRED_RPROVIDER entry to match python-bson
Build Configuration:
BB_VERSION = "1.40.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-16.04"
TARGET_SYS = "arm-linux-gnueabi"
MACHINE = "am437x-evm"
DISTRO = "arago"
DISTRO_VERSION = "2019.07"
TUNE_FEATURES = "arm armv7a vfp thumb neon callconvention-hard"
TARGET_FPU = "hard"
meta-processor-sdk = "HEAD:0d3220f2aa26c6069df78c68bb6009a35067866c"
meta-ros = "HEAD:72068b17e4192b51e09c8dc633805a35edac8701"
meta-arago-distro
meta-arago-extras = "HEAD:9736c7d3e5c4c5a823e9caa712aa27ae24a40e4e"
meta-browser = "HEAD:26d50665e2f7223c5f4ad7481a8d2431e7cb55fb"
meta-qt5 = "HEAD:1520d5b2b2beec5e1c3209d3178219e93ef08bca"
meta-virtualization = "HEAD:7685c7d415e0002c448007960837ae8898cd57a5"
meta-networking
meta-python
meta-oe
meta-gnome
meta-multimedia
meta-filesystems = "HEAD:2d088d252624b19df384aecc434d23afb636178f"
meta-ti = "HEAD:a65f0a338d8f4dcce902cde64fb1413727f1ac20"
meta-linaro-toolchain
meta-optee = "HEAD:615ea7561b844a3867cee4299d83d605c10b02ab"
meta = "HEAD:cd7cf933b3235560ec71576d8f3836dff736a39f"
Initialising tasks: 100% |#######################################################################################################| Time: 0:00:46
Sstate summary: Wanted 6691 Found 0 Missed 6691 Current 112 (0% match, 1% complete)
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: qtdeclarative-5.11.3+gitAUTOINC+e3c0bb7811-r0.tisdk1 do_unpack: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export PATH="/home/ravi/Yocto_Build/tisdk/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/qtdeclarative/5.11.3+gitAUTOINC+e3c0bb7811-r0.tisdk1/recipe-sysroot-native/usr/bin:/home/ravi/Yocto_Build/tisdk/sources/oe-core/scripts:/home/ravi/Yocto_Build/tisdk/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/qtdeclarative/5.11.3+gitAUTOINC+e3c0bb7811-r0.tisdk1/recipe-sysroot-native/usr/bin/arm-linux-gnueabi:/home/ravi/Yocto_Build/tisdk/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/qtdeclarative/5.11.3+gitAUTOINC+e3c0bb7811-r0.tisdk1/recipe-sysroot/usr/bin/crossscripts:/home/ravi/Yocto_Build/tisdk/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/qtdeclarative/5.11.3+gitAUTOINC+e3c0bb7811-r0.tisdk1/recipe-sysroot-native/usr/sbin:/home/ravi/Yocto_Build/tisdk/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/qtdeclarative/5.11.3+gitAUTOINC+e3c0bb7811-r0.tisdk1/recipe-sysroot-native/usr/bin:/home/ravi/Yocto_Build/tisdk/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/qtdeclarative/5.11.3+gitAUTOINC+e3c0bb7811-r0.tisdk1/recipe-sysroot-native/sbin:/home/ravi/Yocto_Build/tisdk/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/qtdeclarative/5.11.3+gitAUTOINC+e3c0bb7811-r0.tisdk1/recipe-sysroot-native/bin:/home/ravi/Yocto_Build/gcc-arm-8.3-2019.03-x86_64-arm-linux-gnueabihf/bin:/home/ravi/Yocto_Build/tisdk/sources/bitbake/bin:/home/ravi/Yocto_Build/tisdk/build/arago-tmp-external-arm-toolchain/hosttools"; export HOME="/home/ravi"; git -c core.fsyncobjectfiles=0 checkout -B 5.11 e3c0bb7811407bad1f65ea55639a4b1d1d39be15 failed with exit code 128, output:
error: packfile /home/ravi/Yocto_Build/tisdk/downloads/git2/code.qt.io.qt.qtdeclarative.git/objects/pack/pack-4cd091cc987792d13111e135adf68988d1b2252a.pack does not match index
error: packfile /home/ravi/Yocto_Build/tisdk/downloads/git2/code.qt.io.qt.qtdeclarative.git/objects/pack/pack-4cd091cc987792d13111e135adf68988d1b2252a.pack does not match index
fatal: unable to read tree 8c7795a587bdc5eab5c881c074cfea51fec2cb07
ERROR: qtdeclarative-5.11.3+gitAUTOINC+e3c0bb7811-r0.tisdk1 do_unpack: Function failed: base_do_unpack
ERROR: Logfile of failure stored in: /home/ravi/Yocto_Build/tisdk/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/qtdeclarative/5.11.3+gitAUTOINC+e3c0bb7811-r0.tisdk1/temp/log.do_unpack.3603
ERROR: Task (/home/ravi/Yocto_Build/tisdk/sources/meta-qt5/recipes-qt/qt5/qtdeclarative_git.bb:do_unpack) failed with exit code '1'
ERROR: qtdeclarative-native-5.11.3+gitAUTOINC+e3c0bb7811-r0.tisdk1 do_unpack: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export PATH="/home/ravi/Yocto_Build/tisdk/sources/oe-core/scripts/native-intercept:/home/ravi/Yocto_Build/tisdk/build/arago-tmp-external-arm-toolchain/work/x86_64-linux/qtdeclarative-native/5.11.3+gitAUTOINC+e3c0bb7811-r0.tisdk1/recipe-sysroot-native/home/ravi/Yocto_Build/tisdk/build/arago-tmp-external-arm-toolchain/work/x86_64-linux/qtdeclarative-native/5.11.3+gitAUTOINC+e3c0bb7811-r0.tisdk1/recipe-sysroot-native/usr/bin:/home/ravi/Yocto_Build/tisdk/sources/oe-core/scripts:/home/ravi/Yocto_Build/tisdk/build/arago-tmp-external-arm-toolchain/work/x86_64-linux/qtdeclarative-native/5.11.3+gitAUTOINC+e3c0bb7811-r0.tisdk1/recipe-sysroot-native/usr/bin/x86_64-linux:/home/ravi/Yocto_Build/tisdk/build/arago-tmp-external-arm-toolchain/work/x86_64-linux/qtdeclarative-native/5.11.3+gitAUTOINC+e3c0bb7811-r0.tisdk1/recipe-sysroot-native/usr/bin:/home/ravi/Yocto_Build/tisdk/build/arago-tmp-external-arm-toolchain/work/x86_64-linux/qtdeclarative-native/5.11.3+gitAUTOINC+e3c0bb7811-r0.tisdk1/recipe-sysroot-native/usr/sbin:/home/ravi/Yocto_Build/tisdk/build/arago-tmp-external-arm-toolchain/work/x86_64-linux/qtdeclarative-native/5.11.3+gitAUTOINC+e3c0bb7811-r0.tisdk1/recipe-sysroot-native/usr/bin:/home/ravi/Yocto_Build/tisdk/build/arago-tmp-external-arm-toolchain/work/x86_64-linux/qtdeclarative-native/5.11.3+gitAUTOINC+e3c0bb7811-r0.tisdk1/recipe-sysroot-native/sbin:/home/ravi/Yocto_Build/tisdk/build/arago-tmp-external-arm-toolchain/work/x86_64-linux/qtdeclarative-native/5.11.3+gitAUTOINC+e3c0bb7811-r0.tisdk1/recipe-sysroot-native/bin:${DEF_TOOLCHAIN_PATH}/bin:/home/ravi/Yocto_Build/tisdk/sources/bitbake/bin:/home/ravi/Yocto_Build/tisdk/build/arago-tmp-external-arm-toolchain/hosttools"; export HOME="/home/ravi"; git -c core.fsyncobjectfiles=0 checkout -B 5.11 e3c0bb7811407bad1f65ea55639a4b1d1d39be15 failed with exit code 128, output:
error: packfile /home/ravi/Yocto_Build/tisdk/downloads/git2/code.qt.io.qt.qtdeclarative.git/objects/pack/pack-4cd091cc987792d13111e135adf68988d1b2252a.pack does not match index
error: packfile /home/ravi/Yocto_Build/tisdk/downloads/git2/code.qt.io.qt.qtdeclarative.git/objects/pack/pack-4cd091cc987792d13111e135adf68988d1b2252a.pack does not match index
fatal: unable to read tree 8c7795a587bdc5eab5c881c074cfea51fec2cb07
ERROR: qtdeclarative-native-5.11.3+gitAUTOINC+e3c0bb7811-r0.tisdk1 do_unpack: Function failed: base_do_unpack
ERROR: Logfile of failure stored in: /home/ravi/Yocto_Build/tisdk/build/arago-tmp-external-arm-toolchain/work/x86_64-linux/qtdeclarative-native/5.11.3+gitAUTOINC+e3c0bb7811-r0.tisdk1/temp/log.do_unpack.3675
ERROR: Task (virtual:native:/home/ravi/Yocto_Build/tisdk/sources/meta-qt5/recipes-qt/qt5/qtdeclarative_git.bb:do_unpack) failed with exit code '
Can you please help in fixing this.
Thanks in advance.
Ravi Kant