Other Parts Discussed in Thread: OMAP-L138, , AM1808
Hi
I have a question about the tool “TI Serial Flasher Host Program for OMAP-L138”.
I would like to program NOR FLASH with AM1806.
To do it, I set the following parameters as:
Target: AM1808 (There is no selection for AM1806, therefore I set AM1808 instead of AM1806)
Device: NOR
The problem is, erase of NOR FLASH is stopped with the message “Waiting for SFT on the OMAP-L138...”
Is there any missing steps?
Thanks
HaTa