Hi
I'd like to confirm if the specific LCDs are available with OMAP-L137.
So, I'd like to send detailed information about LCDs via e-mail.
Please give me feedback if someone is signed to this topic.
Thanks and Best regards,
HaTa.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I'd like to confirm if the specific LCDs are available with OMAP-L137.
So, I'd like to send detailed information about LCDs via e-mail.
Please give me feedback if someone is signed to this topic.
Thanks and Best regards,
HaTa.
Hello,
The Spectrum Digital UI board for the OMAP-L137 EVM comes with a Sharp LQ025Q3DW02 2.5in TFT-LCD panel. Is this what you are looking for?
UI board: http://www.spectrumdigital.com/user-interface-board-for-da830-evm-da830-evm-omap-l137-starter-kit/
UI board documentation: http://support.spectrumdigital.com/boards/assy511240/revc/
Regards,
Sahin
HI
I sent the details information about LCD panels offline.
Please confirm it.
Thanks and Best regards,
HaTa.