Hello TI Experts,
I am trying to capture images from a custom camera module (which is ov5640). I have already used this camera in Linux SDK on my am5728-idk, now I want to use DSP cores and ti-rtos. after some digging in VPS examples, I realized that there is an FVID2 in RTOS which seems to be similar to V4L2 in Linux (correct me if I am wrong). I also can see related files and initializations for ov2659 in "C:\ti\pdk_am57xx_1_0_15\packages\ti\drv\vps\src\devices\ov2659" directory, which seems to be complicated to make it work with ov5640.
now my question is:
Is that possible to configure the VIP and DSS subsystems using FVID2 and camera module using I2C ( to directly write hex values into camera registers) without involving in FVID2 (for the camera part)? if that is possible, please give me some hints on this.
Regards,
Alex.