Other Parts Discussed in Thread: OMAPL138, OMAP-L138, SYSBIOS, SYSCONFIG
Tool/software: Code Composer Studio
hi,
Using Examples by MyExampleProjectsat pdk_omapl138. Regards Example of MCASP_Audio.. example.
The program is inefficient and difficult to decipher. HWI takes 45% cpu and Task 36%.In superficiality the task is copying input buffer to output buffer without any algorithm which in this case gives less than 20% for signal processing.
Is there another example, a simpler one of audio sampling for the LCDKOMAPL138 that can help me?
Thanks,
Itzhak