Part Number: AM3352
Tool/software: Code Composer Studio
Hi
I need to boot device via nandflash,I study the bootloader code,it seems support
DEVICE_ID_FLASH_MT29F2G08ABAEAWP and DEVICE_ID_FLASH_MT29F4G08ABAEAWP,
but my nand is MT29F8G08ABACA .
how can I boot from my own nand?
the pdk version is pdk_am335x_1_0_13,
the nand flash details is :
Device ID : 0xd3
Manufacture ID : 0x2c
Page Size : 2048 Bytes
Spare Size : 64 Bytes
Pages_Per_Block : 64
Number_of_Blocks : 8192
Device_width : 1 Byte
DeviceSize : 1024 MB