Other Parts Discussed in Thread: SYSBIOS
Hello,
I have initialized clock in following way:
============================================================
Here is the function, which checks whether the timer parameters has changed. I am using timer and clock API functions int one place. It is causing errors.
============================================================
error: a value of type "ti_sysbios_knl_Clock_TimerProxy_Handle" cannot be used to initialize an entity of type "ti_sysbios_hal_Timer_Handle"
during compilation.
[HOST] [IPU2 ] 12.864789 s:
[HOST] [IPU2 ] 12.864820 s: ### XDC ASSERT - ERROR CALLBACK START ###
[HOST] [IPU2 ] 12.864881 s:
[HOST] [IPU2 ] 12.865033 s: E_hardFault: FORCED
[HOST] [IPU2 ] 12.865094 s:
[HOST] [IPU2 ] 12.865125 s: ### XDC ASSERT - ERROR CALLBACK END ###
[HOST] [IPU2 ] 12.865186 s:
[HOST] [IPU2 ] 12.865399 s:
[HOST] [IPU2 ] 12.865460 s: ### XDC ASSERT - ERROR CALLBACK START ###
[HOST] [IPU2 ] 12.865521 s:
[HOST] [IPU2 ] 12.865643 s: E_busFault: PRECISERR: Immediate Bus Fault, exact addr known, address: 119395cc
[HOST] [IPU2 ] 12.865735 s:
[HOST] [IPU2 ] 12.865765 s: ### XDC ASSERT - ERROR CALLBACK END ###
[HOST] [IPU2 ] 12.865826 s: