Other Parts Discussed in Thread: PROFIBUS
Tool/software: TI C/C++ Compiler
I was working with profibus example I can loading via debugger and make testing
I use sys_bios _SDK industry example
But when I loading by mistake I make reset board at same time
After that .......
Unfortunately. .flash has erase and when I make loading example I get this error
Value at address 0x80000002 donot match please Verify target memory and memory map .
I try to fash this bootloader
dslite. bat --mode processors -come -f C:ti\pdk_am335x_1_0_6\packages\ti\startware\binary\bootloader\bin\am335x_evm\gcc\bootloader_boot_mcspi_a8host_debug_ti. bin
But cannot flashing
Also ...
İ could Flash Project via spi_flashing_tool
But now I can not ....!!!!!!
İ Check memory browse at 0x8000002 to 0x8ffff
All is zero
Please any one help me ..