Other Parts Discussed in Thread: TMDSEMU110-U
Tool/software: Code Composer Studio
Hi TI suppoters,
I tried to connect embedded XDS100 JTAG on EVM5517 to an external C5517 processor.
This processor is already supplied power and clock.
I also connected the Reset pin of the processor to the Reset signal (Pin number 2 of JP3) on EVM5517 board.
The boot mode of the processor is set to Zero (Boot from NOR FLASH).
I tried to connect to processor from CCS but below error occurred and can't connect to it.
Therefore, I would like to confirm if I can use embedded XDS100 JTAG on EVM5517 to connect and debug software on an external C5517 processor.
If yes, how can I make a correct connection ?
Thank you and best regards,