This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDEP-01017: MMWCAS-DSP-EVM unresponsive after connecting to MMWCAS-RF-EVM with AWR2243 chips

Part Number: TIDEP-01017
Other Parts Discussed in Thread: AWR2243, MMWCAS-RF-EVM, MMWCAS-DSP-EVM, AWR1243

I recently bought a MMWCAS-DSP-EVM & MMWCAS-RF-EVM combination. The MMWCAS-RF-EVM is populated with AWR2243 chips. When I connected the boards and powered them on, only 1 LED came on and the MMWCAS-DSP-EVM board is unresponsive through the serial port.

We have another set of these 2 boards but the MMWCAS-RF-EVM is populated with AWR1243 chips. When I plug in this board stack multiple LEDs are illuminated (e.g. 3 & 5V Power Good LED, etc) and I can access the Arago OS command prompt through the serial port.

Is the set of boards I just received from TI damaged? Does connecting the MMWCAS-RF-EVM populated with AWR2243 chips cause a short on the MMWCAS-DSP-EVM board? I have tried using the MMWCAS-DSP-EVM with and without the MMWCAS-RF-EVM connected and the behaviour is the same.