Other Parts Discussed in Thread: PROFIBUS,
Hi,
EVM board: iceAMIC110
SDK: PRU-ICSS-Profibus_Slave_01.00.02.01
The customer ran Profibus slave demo and console display below menu:
Profibus Application Running...
I - Change inputs
S - Send static diagnosis
C - Clear diagnosis
E - Send ext. diagnosis
D - DP Status
P - Print Menu
When he input S or E, he could not receive diagnosis data, which port is used to receive the corresponding diagnosis data?