Other Parts Discussed in Thread: OMAP-L138, AM1808, AM1810, OMAPL138
Hello,
We are developing an application for the C6742 DSP which will have an external EMIF-NOR as flash device to store the application binary. The setting we are testing our code on right now is the C6748 DSP Development Kit. We have successfully flashed the application and boot it from both the NAND flash the LCDK comes with, and also from an external custom NOR board interfacing with EMIF. In both cases we used sfh_OMAP-L138 application.
From the sfh_OMAP-L138 documentation, the target flag can be set to: OMAPL138, OMAPL138_LCDK, AM1808, AM1810, C6748, C6746, C6748_LCDK (default is OMAPL138). The flag we have been using so far is "C6748_LCDK". Nevertheless, I have seen in this post that this serial flashing utility can also be used to flash a binary application for a C6742 DSP. ¿Is this correct?
If so, considering that BOOT pins are set to the correct setting in the C6742 DPS board to boot from UART0, that is: BOOT[7:0] = [0001 0110] (taking into account that default baud rate is maintained by BOOT[7:5] = 000), ¿which flag should I use when flashing the C6742 DSP based board? ¿Would it work with C6748 flag instead of C6748_LCDK?
Thanks in advance,
David