Part Number: AM3358
Dear Support Team,
could You please confirm, if below 2 use cases can be addressed with AM3358 device?
- AM3358 device should be able to get data over SPI and transfer data over its USB interface to a USB stick for data storage … basically a SPI-2-USB bridge functionality
- The same USB slot should be able to be used as a USB charging port for other devices e.g. Smartphone with up to 1.5A charging current for the case when above mentioned USB stick from 1) is not plugged in for example
From the Datasheet, TRM and reference design ( http://www.ti.com/tool/TIDEP0013 ) I understand, that it should be possible, if using a different power switch allowing more than 1.5A, correct?
Many thanks and best regards,
Gregor