Hi,
On a current custom design based around the C5515, the DVDDEMIF is set to 3.3V and the EMIF is configured for use with a 3.3V compatible SDRAM from ISSI.
After having discussed with ISSI apps engineers regarding lowering memory power consumption, they advised lowering SDRAM power consumption through lower memory supply, and we all agree it is the best overall means to reduce SDRAM power drain.
If this is the case, from a board redesign perspective, is there anything else one would need to modify to the existing board, other than to set all processor DVDDEMIF power pins to a suitable 1.8V (or 2.5V), and then replacing the existing 3.3V SDRAM device with an equivalent lower voltage type ? I would envisage the register configuration to otherwise remain unchanged...
Thanks in advance for your advice, regards,
MM