Yesterday, while I was working on C5517 evaluation board (TMDSEVM5517), there has been some smell of burning from the board. I’ve immediately turned it off.
I switched it on today, but the on-board USB emulator fails in connecting to the board.
Furthermore, the voltage on J10 header is 1.5V on pin 9 (rather than 3.3V), and 0.5V on pin 7 (rather than 1.8V).
Is there something I may try to locate the failed component(s) ?
Thanks,
Aldo Minardo