This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSLCDK138: DSP Kit with Colored-LCD capacitive touch screens

Part Number: TMDSLCDK138
Other Parts Discussed in Thread: OMAPL138

Hi Team,

Our customer reached us out asking for our solution for their ECG/EEG application. After a couple of correspondence we've closed quite of their request regarding the input and data conversion block of the application. Part of their request is a processing core that can perform FP calculations. We've proposed our L138/C6748 development kit but one of their critical requirement is the compatibility with an LCD capacitive touch screen. The CircuitCo ULCD7 Lite LCD for L138 is quite old and our customer is having hesitations to go with this kit if it is only LCD that can be used with it.

Can you advise if there are any newer LCD screens that can be used with the kit? If we have other FP DSP kit(s) that could be an option we would gladly look into it as well. Thanks in advance.

Kind Regards,

Jejomar

  • Jejomar,

    Sorry for the delay in responding. Unfortunately there are no newer LCD screens that have been currently tested with this LCDK kit. The OMAPL138/C6748 Logic PD EVM (currently EOL) was the only other option available with LCD support for development with this device.  

    The LCDK VGA connector has been tested for display if that options works for the customer. 

    Regards,

    Rahul