Other Parts Discussed in Thread: MMWCAS-DSP-EVM, MMWCAS-RF-EVM
We recently bought a MMWCAS-DSP-EVM & MMWCAS-RF-EVM combination.
When we connected the boards and powered them on, only the Input
12V Power Indicator LED came on and the MMWCAS-DSP-EVM board was
unresponsive through the serial port.
The 5V test point (SYSTEM_5V0, TP41/TP43) is only reading 1.4V.
The behaviour is the same with and without the MMWCAS-RF-EVM connected.
We use a Bicker BET-0612 12V/5A power supply.