Hello,
I know this information has to be somewhere in the user manual but i can't quite find it. I am testing RAM using a GEL File script via CCS. I am doing a WR_MEM_32 and then reading it back with RD_MEM_32. On one of my boards my second-most least significant Byte is bad (i.e. i write 0x00000000 and i read back 0x0000ZZ00 where ZZ is some non-zero value). I have 4 DDR chips connected to the BUS 1 for each byte, I am trying to figure out which chip that is associated to so i can investigate more but am not sure what order the Data Macros are sending out the bytes. Is the messed up byte in my scenario DDR D23:16 OR D15:8?
Thanks,
Jarrod