Hi,
What is the output voltage of the GPIO pins on the DM3725? Is it possible to configure them to 3.7V?
Thanks,
Joseph
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
What is the output voltage of the GPIO pins on the DM3725? Is it possible to configure them to 3.7V?
Thanks,
Joseph
No.
The datasheet defines two operating voltage ranges for dual-voltage IOs, 1.71V to 1.91V for a nominal 1.8V operating condition, and 2.7V to 3.6V for a nominal 3.0V operation condition. So a potential of 3.7V would exceed the recommended operating conditions of the device.
Regards,
Paul