In the example of Cascade_radar_beam_form, the following error occurred when modifying the Chirp parameter to set the sample points to 512
[IPU1-0] 14.243518 S: CAPTDRv/SRC/VPSDRV_capturecore.c@line 643:
[IPU1-0] 14.243610 s: Core control: Set Max Frame Size failed
[IPU1-0] 14.243701 S: Line: 395 in capturelink_drV. C: Status == FVID2_SOK: Failed!!
The setting of sample points to 511 can be set successfully, I have read the documentation and forums and mentioned that the maximum number of sample points is 512, and why the example of Cascade_radar_beam_Form sets the sample points to 255 instead of 256, and The example of Cascade_radar_object_detect to 256
However, with the same configuration parameters, I used mmWavestduio to configure successfully and collect ADC data