Other Parts Discussed in Thread: TMS320DM6467T
This should be a fairly simple question, and I beleive the answer is no - but I want to confirm because it would be much easier if the answer was yes - does the dm6467 support jumbo packet sizes? And if yes, what do I need to change to do that? right now I am developing on the TMS320DM6467T and I see that if I change the mtu on my host machine, the nfs share with the evm will "break". When I change the mtu back to 1500, nfs is ok. Also, changing the mtu on the evm does not seem to have an effect either way.
Thanks for your help, I expect this should be an "easy one".
Brandy