Tool/software: Code Composer Studio
Hi,
The TMS320C5505 data sheet shows that the maximum operating frequency of EM_SDCLK is 50 MHz when DVDDEMIF = 1.8 V, as shown in the figure below.
Does this mean that the operating frequency of the DSP needs to be less than 100 MHz?
This provision seems to have been added from Rev. F of the DS, what is the reason for this condition being added?
My customer adopted the C5505 before this requirement was stipulated. There is mSDRAM connected to EMIF and it is run on EMIF_CLK of 100Mhz and above.
This is why it is a major problem. So, I would like to clarify why this condition has been added.
Best Regards,
H.U