Part Number: 66AK2H06
Hi Tom,
I got additional question for K2H USBCLK.
According to previous discussion,
- USB SerDec IP is not the same as other SerDes
- There is no internal termination circuit
Customer added an external termination 100-ohm resistor and signals are AC coupled with 0.1uf.
According to Hardware Design Guide (SPRABV0) table 6, USB requires AC coupling.
Below waveform is observed on customer board (USBCLKP).
As you can see the signal is 0V centered (no DC offset). Is this expected?
The low side is close to Absolute Maximum Rating for SerDes Input (-0.3V)
For comparison, PCIECLKP and SYSCLKP waveforms are below.
All three clocks are provided the same LVDS driver.
AC coupling is really required for USBCLK?
Thanks and regards,
Koichiro Tashiro