Other Parts Discussed in Thread: OMAP-L137
I have problems with booting from flash using the Processor SDK RTOS 06_03_00_106 documentation.
I got this error using the spi_flash_writer.out from Processor SDK RTOS 06_03_00_106:
*** PDK SPI Flash Writer ***
Opening SPI handle...
SPI init failed!
I got this error using the original spiflash_writer.out, where I can set the offsets of the MLO (0) and app (0x80000):
**** PDK SBL ****
SBL Revision: 01.00.09.02 (Sep 30 2020 - 17:12:59)
Begin parsing user application
Invalid magic number in Single image header
Jumping to user application...
I've checked the header of the app file and it has the magic number:
4d 53 54 52 01 20 20 20 37 20 20 20 20 20 20 20 20 20 20 20 20 20 20 20 20 20 20 20 4d 45 4e 44
My conclusion is that the 0x80000=524288 offset in flash (MLO offset=0, app offset is 0x80000) is not correct in MLO.
Can somebody confirm this?
Thanks