Hi fellows,
the TRM of the 66AK2Gx states the following:
"The Quad Serial Peripheral Interface (QSPI™) module is a kind of Serial Peripheral Interface (SPI) module which allows single, dual or quad read and write access to external flash devices" (Page 3965)
So my question is, can the QSPI be used for communication between other devices (e.g. two SoCs) than memory devices?
The idea is to connect two EVMK2GX evaluation boards so that they can communicate via QSPI. However, from the schematics it seems that this is not possible.
But from my point of view at least the SoC should be capable of it.
Best Regards