Other Parts Discussed in Thread: OMAP-L137
We need to clarify a question about boot mode.
Our schematic design configures Boot Mode pins in "SPI0 Flash" mode.
For emulation purpose (JTAG with XDS200) is it necessary to provide alternative boot mode configurazione as in the picture? Or the connection with emulator is always available (as it seems to me).
We ask because it is not good to have a strong pull-up/pull-down to provide two alternative boot modes on a very fast SPI port.
On the OMAP-L137 EVM, the emulator can connect in any boot configuration except "SPI0 Flash"; but in "SPI0 Flash" linux OS on ARM starts and maybe it freeze the DSP chip....