This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA746: can I replace pin2pin DRA744 with DRA746 ?

Part Number: DRA746
Other Parts Discussed in Thread: DRA744,

HI everybody ,

please  can I replace  DRA744BJGABCRQ1  with  

DRA746PPIGABZRQ1 ? are they pin2pin ?

only difference I can see is  package  thickness , anything else ?

for sure I ll check  PMIC  consumption ...

thnak you 

best regards

Carlo

  • Carlo,

    The DRA744 and DRA746 are the same device and are pin to pin compatible.  The only difference is that the DRA746 MPU is capable of running at 1.5 GHz compared to 1.0 GHz for the DRA744.  The power on the DRA746 is higher than the DRA744, so a different PMIC mapping may be needed.

    Regards,

    Kyle