Other Parts Discussed in Thread: SYSCONFIG
Hi all,
I have a DRA726 with the following unused balls:
I've followed the "Unused Balls Connection Requirements" section in DRA726 datasheet and while everything is crystal clear in the HW side, I have some doubts in the SW side regarding the following note:
"All other unused signal balls with a Pad Configuration register can be left unconnected with
their internal pullup or pulldown resistor enabled"
I've seen SysConfig generates the required config files regarding the USED balls, but it does not generate any output file regarding the UNUSED ones. So.. How I'm supposed to configure the PU/PD of the unused balls, like ON_OFF?
- Should I configure the unused balls on the fly while the DRA is booting?
- Should I set up the peripherals I won't use in SysConfig the same way I configure the ones I'use to include them in the output files?
Thank you very much in advance!