Customer wants to use byte-mode to save memory, but I see in compiler readme only C55+ core support byte-mode, but did not say which device is C55+ core
In C5505 datasheet, the CPU is V3.3, not mention plus, which device used C55Plus core?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Customer wants to use byte-mode to save memory, but I see in compiler readme only C55+ core support byte-mode, but did not say which device is C55+ core
In C5505 datasheet, the CPU is V3.3, not mention plus, which device used C55Plus core?
Hi Tony,
According to this E2E thread,
The C55+ CPU was not available on any Catalog product - it was only used on certain custom devices under NDA.
Regards,
Sahin