This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6657: timer period in external clock mode

Part Number: TMS320C6657

Hello

I am using external clock mode in TMS320C6657 timer. The clock input on TINPL pin is 10K in frequency, and I would like to generate a timer event, such as TINT2L, in same frequency.  

In this case, how to setup the timer period? when I set PRDLO to 1, the TINT2L is generated in 5K frequency. While, when I set PRDLO to 0, no TINT2L timer interrupt is generated. 

How to create the same frequency interrupt as that on the TINPL input?  Thanks!