Team, can you please help address the issue my customer is having:
I want to debug a bootloader program that is going to run in a C6713 DSP. As far as I know, the DSP copies 1 kB from flash to IRAM during boot. This bootloader program would contain 1 kB sized code section which is the responsible to copy the rest of the program from flash into RAM. This should be no problem at all with production builds, but during the debugging process I have a problem.
Currently, the linker command file is defining the memory sections with origin in flash and to run in RAM. However, the CCSv5 debugger is not able to load the program sections that should be inside the flash, BUT it can do for memory sections in RAM. This makes the process of debugging the bootloader quite more uncomfortable, because for each debug session after change in the code, I need to reopen Flashburn, run, erase and burn. So my question here is why is the CCSv5 not able to load the program in flash memory while it can do in the other memories (both internal and external RAM) and how I can fix it so I can simplify the debug process of a bootloader program that copies from flash into RAM. If it helps, I am using a DSK6713 development board with the CCSv5 and the Blink example that comes with the Flashburn software.
Customer's project can be made available off-line.
Thanks
Viktorija