Other Parts Discussed in Thread: SYSBIOS
Hi,
I'm using OMAP l138. Project build on ARM with sysbios_6_76_03_01 and RTOS. The USB0_ID state is switched with GPIO. When I initialize USB0 as host (USB0_ID pulled to ground) , USB0_DRVVBUS switches to 1, Session bit also to 1 and 5V appears on port. But when I plug in usb flash, iterrupts 'DRVVBUS level change' and 'VBUS lessthen VBUS valid' appear , USB0_DRVVBUS switches to 0 and and after usb_reset_event SB0_DRVVBUS back to 1 , but then nothing happens.
Any help is really appreciated.
Best Regards
Dmitriy