Part Number: OMAP3530-HIREL
Hello Guys,
Good day.
Just like to clarify. On page 256 under device nomenclature of the device it was stated that the 'A' suffix means it is rated at -40° C to 105° C. However, on the Packaging information on page 258, all orderable part numbers are rated at -40° C to 105° C despite the absence of the 'A' suffix.
Which if this is right?
Thanks in advance!
Art