This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3530-HIREL: Temperature Code clarification

Part Number: OMAP3530-HIREL

Hello Guys,

Good day.

Just like to clarify. On page 256 under device nomenclature of the device it was stated that the 'A' suffix means it is rated at -40° C to 105° C. However, on the Packaging information on page 258, all orderable part numbers are rated at -40° C to 105° C despite the absence of the 'A' suffix.

Which if this is right?

Thanks in advance!

Art

  • Art

    I believe the Packaging Information table on page 258 is incorrect.   Only the "A" temperature grade parts are -40C to 105C.

    I'll get the team to correct this issue. 

    Thanks for highlighting this. 

    --Paul