Other Parts Discussed in Thread: TMDSEVM6657, TIDEP0036, TMS320C6657
Hi experts,
My customer is using TMS320C6652 for their design and they are comparing it with TMDSEVM6657 as they go along. Please let me know about the following questions.
(1) Regarding the number of board layers, is it correct to assume that 6 layers will not be a problem?
"6.3.1.2 Stack Up - SDRAMs" in "DDR3 Design Requirements for KeyStone Devices (Rev. C)" recommends a minimum of 8 layers if the board area is large. The TMDSEVM6657 schematic has 12 layers, but they don't think it's necessary for this board (C6652 board) (based on the customer's circuit size).
(2) Regarding the control sequence of the power input and reset signal at startup, is it correct to assume that the parts that do not have a time specification are fine as long as the order is followed?
There are many parts in the datasheet "6.3.1 Power-Supply Sequencing" that do not have a time limit. For example, CVDD1 is described as "at the same time or shortly following CVDD", but we could not determine how much time it should be.
(3) After the input of CVDD and CVDD1, there is a period of tens of seconds when the clock input is not stable before the input of CVDD18. Can I assume that this is not a problem?
According to "6.3.1.1 Core-Before-IO Power Sequencing", there is no problem even if the clock is unstable during the period between CVDD1 and CVDD18 inputs or during the "Power Stabilization Phase". I would like to confirm this just in case. If there is a problem, it would be helpful if you could tell me what kind of processing is needed on the clock input pins.
Best regards,
O.H