I am trying to use DSP/BIOS on TMSDSK6416 with CCS compiler version v6.1.3. I have installed the following products:
1) DSP/BIOS version v6
2) xdcTools version 3.3
3) SYS/BIOS version 6.46
I am added the environment variables and the path as stated in the setup guide of DSP/BIOS.
I am encountering an issue regarding accessing the implicit DSP/BIOS instrumentation tools for instance, CPUload graph, Execution graph etc. The tools aren't showing on the file handling tab. Whenever I access the analysis tools, an error occurs regarding the valid UIA configuration file. I am attaching the screeenshot of the error. My question is that, is the issue regarding the compatibility of the DSP/BIOS version with the compiler version? Or is the CCS not discovering the installed tools?
Currently, I am executing DSP/BIOS examples and would like to analyse the results.