hi experts,
My customer has created a project for C6713 in CCS v3.1 and is trying to migrate it to CCSv10.x using the following information.
・Importing CCSv3.3 Project to CCS Eclipse
Q1: They were originally built with COFF, but now they are trying to change to ELF. Could you please share the migration guide from COFF to ELF for C6000 like the following information?
・C2000 Migration from COFF to EABI
The above is for C2000, but I believe most of it is applicable to C6000 as well. Also, I found the following document, but the link "">processors.wiki.ti.com/.../C6000_EABI_Migration." is broken because it refers to the TI-Wiki content The link is broken.
We have told our customers that if they use compiler v7.4.24 and do not need the ELF feature, they can use COFF. However, they want to change to ELF, so it would be great if you could share some helpful information.
Best regards,
O.H