While using the Google search about programming of 6713 dsk through code composer studio. I came across multiple header files especially ''csl.h '' and "ledcfg.h'
?
What are the application scenarios of these two header files?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
While using the Google search about programming of 6713 dsk through code composer studio. I came across multiple header files especially ''csl.h '' and "ledcfg.h'
?
What are the application scenarios of these two header files?
Hi,
The Chip Support Library (CSL) provides an application programming interface (API) used for configuring and controlling the DSP on-chip peripherals for ease of use, compatibility between various C6000 devices and hardware abstraction. This will shorten development time by providing standardization and portability. The functions listed in the features section are specifically designed for the following devices: C6201, C6202, C6203, C6204, C6205, C6211, C6410, C6412, C6413, C6414, C6415, C6416, C6418, C6701, C6711, C6712, C6713, DA610, DM640, DM641 and DM642.
I can't comment on the ledcfg.h as this is not the standard CSL h file from below.
Hope this resolves your question on CSL.