Hi,
Ti-sdk version: ti-processor-sdk-linux-am335x-evm-06.03.00.106
U-Boot Version: U-Boot 2019.01-gc148924
USB Devices:
+ 2.5" external SATA drive with SATA to USB interface ( JM20329,MA6116A )
At the U-Boot shell, the above device was not detected when I connected them to USB PORT on Beaglebone Black.
USB Storage devices viz. Western Digital Portable Drive (My Passport) were detected properly by the same Beaglebone Black.
For the USB devices failing to be detected, I get only a "Port Not Available" message.
Is this behaviour expected ?? and how do I overcome this?
Regards,
Adarsh