Part Number: TMDX654GPEVM
Hello,
I have a TMDX654GPEVM (HW REV 1.0) with a PCIe custom board connected to the SERDES X1 connector.
I can correctly see the PCIe device with `lspci` command using Arago standard image flashed from the offical SDK (version am65xx-evm-06.01.00.08) that came with the board.
Output of `lspci` consisted of two recognized devices: the first is the onboard controller and the second was my custom card.
After upgrading to PROCESSOR-SDK-LINUX-AM65X 07_01_00_17 and flashing the standard image (with mksdboot.sh with PG1.0 sysfw command line switch) I cannot see the PCIe devices anymore.
Output is empty.
Also, in kernel boot log there is not evidence of PCIe devices enumeration.
I see that in errata and known issues there are a few references to PCIe:
Could you please help me fixing this issue?
Best regards