Hello,
I am using K2G keystone, on eval board 66AK2GG1. Using TI Linux SDK 06_03_00_106, I am loading the kernel with arago-base-tisdk-image rootFS.
I would like to load DSP, but I notice there is no MPM (client nor Server) applications/libraries inside the file system. I followed http://software-dl.ti.com/processor-sdk-linux/esd/docs/latest/linux/Overview_Building_the_SDK.html, and rebuild the SDK file system. I have also recompiled using bitbake multiprocmgr.
I am now looking to install the IPK into the FS on the target. I am wondering if you have a list of IPK I shall install and more importantly the configuration that are needed to start the server.
Also is there another way to load the DSP code ?
Thank you for your help,
Cheers,
Vincent