Hello,
I am curious as to what the meaning of the linker error permission denied can be interpreted to mean.
I am working on a project where I have exchanged an older version of the NDK and its associated libraries for
the newer NDK 2.25.1.11 and its associated libraries.
The project compiled and linked successfully with the older NDK and labraries.
After adding the newer version it fails due to a linker error stating "Permission Denied"
The exact error message is below:
#6001 cannot open file "C:/DRT1000/FreshSvnDownload/SDK/Platform_Adaptation_Library/AFM_ASP/drt-ipc/packages": Permission denied
I have checked permissions on the file folder and have verified that I have read/write/modify privileges there.
This folder is the same folder from the earlier project which compiled and linked successfully.
Is there a list of items I should be running through as a result of seeing a permission denied error in general?
Thank You,
Forrest