This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

UART BOOT doesn't working

Genius 3220 points

Replies: 11

Views: 1352

Hi,

I have verify that the uart boot is successful on the evm board. (dra742)

but I failed when I tried to verify uart boot on our previous generation product. (dra744)



1st stage boot to MLO is working and the command line shows "u-boot-spl.bin file download completed.

then I try to  transmit u-boot.img to DUT through YMODEM, but it's can't working. XMODEM also.

Are there any hardware settings that need to be changed?

thanks for your help

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.