This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

Linux/AM4378: Spidev does not output on pins

Intellectual 610 points

Replies: 25

Views: 8713

Part Number: AM4378

Tool/software: Linux

Hi Everybody!

I recently got my spidev devices registered in /dev (see here for details). 

My devices don't seem to work unfortunately.  I have only scoped out spidev1.1 so far.  I can open the device.  When I configre it I do get messages complaining about not using DMA (see below).  And then I get a TXS timed out message.

I am using a program really similar to this one.  I just added a ton of printing and slowed things down so that I could tell which actions were causing the system log messages.

Here is the output.

root@am437x-evm:/ace/bin# ./helloSpi -C 301
helloSpi ...
    ...Options selected
        device = /dev/spidev1.1
        speed = 24000000
        delay = 0
        bits = 8
        mode = 0x04
    ...Creating device
    ...Setting SPI option
    ...Opening file handle
    ...Committing options     <-- 3 ioctl calls in here
[62332.673461] spidev spi1.1: not using DMA for McSPI (-19)
[62332.678907] spidev spi1.1: not using DMA for McSPI (-19)
[62332.689027] spidev spi1.1: not using DMA for McSPI (-19)
    ...Setting up data transfer
        TX = 0x03 0x01 0x00 0x00 0x00 0x00 0x00 0x00
        RX = 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00
    ...Performing ioctl data transfer   <-- 1 ioctl call in here
[62340.712144] spidev spi1.1: TXS timed out
    ...Receive buffer
        RX = 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00
Good bye!

I had our electrical team scope the clk, miso, mosi, and cs pin for spidex1.1 and there is no activity.

I also see the cs pin held low the entire time.  I think it should only go low when the spi master wants to send data to or retrieve data from that particular device.

Here is my pin mux...

spi2_internal_pins_default: spi2_internal_pins_default {
    pinctrl-single,pins = <
        0x260 ( PIN_OUTPUT | INPUT_EN | MUX_MODE0 ) /* (N20) spi2_sclk.spi2_sclk */
        0x264 ( PIN_OUTPUT | MUX_MODE0 )            /* (P22) spi2_d0.spi2_d0 */
        0x268 ( PIN_INPUT_PULLUP | MUX_MODE0 )      /* (P20) spi2_d1.spi2_d1 */
        0x1b0 ( PIN_OUTPUT | MUX_MODE4 )            /* (AE17) cam0_hd.spi2_cs1 */
        0x1c4 ( PIN_OUTPUT | MUX_MODE4 )            /* (AB19) cam0_data8.spi2_cs2 */
    >;

}

&spi2 {
    compatible = "ti,omap2-mcspi";
    pinctrl-names = "default";
    pinctrl-0 = <&spi2_internal_pins_default>;
    status = "okay";

        ti,spi-num-cs = <4>;
        ti,pindir-d0-out-d1-in = <1>;

ksz8895@1 {
    compatible = "rohm,dh2228fv";
    spi-max-frequency = <100000>;
    reg = <0x1>;
    status = "okay";
    #address-cells = <1>;
    #size-cells = <0>;
};
ksz8895@2 {
    compatible = "rohm,dh2228fv";
    spi-max-frequency = <100000>;
    reg = <0x2>;
    status = "okay";
    #address-cells = <1>;
    #size-cells = <0>;
};

};

Here are (what I think are pertinent) defconfig settings. In fact here's everything SPI related.  I highlighted the ones I think actually matter

root@am437x-evm:/ace/bin# cat /proc/config.gz|gunzip|grep SPI|grep \# -v|grep SPIN -v
CONFIG_REGMAP_SPI=y
CONFIG_MTD_SPI_NOR=y
CONFIG_SPI_CADENCE_QUADSPI=y
CONFIG_WLCORE_SPI=m
CONFIG_INPUT_ADXL34X_SPI=m
CONFIG_SPI=y
CONFIG_SPI_MASTER=y
CONFIG_SPI_BITBANG=m
CONFIG_SPI_GPIO=m
CONFIG_SPI_OMAP24XX=y
CONFIG_SPI_TI_QSPI=y
CONFIG_SPI_SPIDEV=y
CONFIG_SND_SOC_I2C_AND_SPI=y
CONFIG_RTC_I2C_AND_SPI=y

I've seen various posts about differing pinmux settings.  I've seen Biser say the clk needs to be an input (I tried, no change), I've seen another post that said they had success with clk as output with input_en flag.  So I'm not sure what is the "right" answer. 

All thoughts/suggestions/troubleshooting tips are welcome.

Thanks in advance!

Nathan

  • Hi,

    Which SDK are you using?

    Best Regards,
    Yordan

     


     Please make sure you read the forum guidelines first.

  • Looking at am43xx.h it appears output & input_en is the same thing as input...

    #define PIN_OUTPUT (PULL_DISABLE)

    #define PIN_INPUT (INPUT_EN | PULL_DISABLE)

    ...so both are the right answer.

  • In reply to Yordan Kovachev:

    Linux SDK 4.
  • In reply to Nathan Wright:

    Hi,

    Try these settings for enabling the SPI:
    e2e.ti.com/.../2321156

    The post is for am335x, but the general pinmux settings (only register addresses and muxmodes may differ) & SPI settings are the same for all Sitara devices.

    Best Regards,
    Yordan

     


     Please make sure you read the forum guidelines first.

  • In reply to Yordan Kovachev:

    Hi Yordan,

    Thanks for your help.  I tried the settings in the post you referenced and I have made incremental progress.  The chip select lines are now high when inactive.   I still do not see any activity on the SPI bus when attempting a read of the slave device.

    dts state now...

    spi2_internal_pins_default: spi2_internal_pins_default {

    pinctrl-single,pins = <

    0x260 ( PIN_INPUT | MUX_MODE0 ) /* (N20) spi2_sclk.spi2_sclk */

    0x264 ( PIN_OUTPUT | MUX_MODE0 ) /* (P22) spi2_d0.spi2_d0 */

    0x268 ( PIN_INPUT | MUX_MODE0 ) /* (P20) spi2_d1.spi2_d1 */

    0x1b0 ( PIN_OUTPUT | MUX_MODE4 ) /* (AE17) cam0_hd.spi2_cs1 */

    0x1c4 ( PIN_OUTPUT | MUX_MODE4 ) /* (AB19) cam0_data8.spi2_cs2 */

    >;

    };

    &spi2 {

    compatible = "ti,omap2-mcspi";

    pinctrl-names = "default";

    pinctrl-0 = <&spi2_internal_pins_default>;

    status = "okay";

    ti,spi-num-cs = <4>;

    ti,pindir-d0-out-d1-in = <1>;

    ksz8895@1 {

    compatible = "rohm,dh2228fv";

    spi-max-frequency = <100000>;

    reg = <0x1>;

    status = "okay";

    #address-cells = <1>;

    #size-cells = <0>;

    spi-cs-high;

    };

    ksz8895@2 {

    compatible = "rohm,dh2228fv";

    spi-max-frequency = <100000>;

    reg = <0x2>;

    status = "okay";

    #address-cells = <1>;

    #size-cells = <0>;

    spi-cs-high;

    };

    };

    Interestingly, I do see a spurt of traffic on start up.  I think u-boot might be probing it, and then perhaps the kernel does aswell?  Could there be some other driver getting in the way of spidev?

  • In reply to Nathan Wright:

    Hi Nathan,
    I was working on AM335X SPI three years back. I had to configure SPI CLK as INPUT to get SPI to working state. Check whether this works for you. Also check whether your MOSI and MISO lines are configured correctly. Find out if there is any restriction on MOSI and MISO to be configured in particular way.

    Regards,
    Gangadhar

  • In reply to Nathan Wright:

    Hi,

    I just noticed the following:
    ksz8895@1 {
    compatible = "rohm,dh2228fv";
    ksz8895@2 {
    compatible = "rohm,dh2228fv";
    KSZ8895 are network devices, that are NOT supported by the spidev driver (rohm,dh2228fv). You should connect them to MII/RMII interface.

    Also for debug purposes can you try to read the pinmux registers with devmem2 to see if they have the values passed from dts? As a suggestion try adding the pinmux configurations in u-boot as well. In latest SDKs pinmux is done in u-boot.

    Best Regards,
    Yordan

     


     Please make sure you read the forum guidelines first.

  • In reply to Yordan Kovachev:

    Thanks Yordan,

    We are not using the SPI interface to these switches for network traffic.  We simply intend to configure them and gather port statistics and such.  I think the spidev driver will work for this.  I'm simply implementing table 4-1 of this datasheet.

    On devmem2, what memory address should I be reading?  I tried reading spi2 address from am4372.dtsi (0x481a2000) but devmem2 core dumped.  Here is the output...

    root@am437x-evm:~# devmem2 0x481a2000
    /dev/mem opened.[61703.934441] Unhandled fault: external abort on non-linefetch (0x1018) at 0xb6f2f000
    [61703.943222] pgd = ed628000
    [61703.945950] [b6f2f000] *pgd=fc99f831
    [61703.949715] ------------[ cut here ]------------
    [61703.954406] WARNING: CPU: 0 PID: 810 at drivers/bus/omap_l3_noc.c:147 l3_interrupt_handler+0x25c/0x36c
    [61703.963773] 44000000.ocp:L3 Custom Error: MASTER M2 (64-bit) TARGET L4_PER_0 (Read): Data Access in User mode during Functional access
    [61703.975917] Modules linked in: bc_example(O) xhci_plat_hcd xhci_hcd usbcore dwc3 udc_core usb_common ti_am335x_adc sha512_generic sha512_arm s)
    [61704.023348] CPU: 0 PID: 810 Comm: devmem2 Tainted: G W O 4.9.28-geed43d1050 #24
    [61704.031659] Hardware name: Generic AM43 (Flattened Device Tree)
    [61704.037611] Backtrace:
    [61704.040129] [<c010b7d0>] (dump_backtrace) from [<c010ba8c>] (show_stack+0x18/0x1c)
    [61704.047754] r7:00000009 r6:00000000 r5:c09b3204 r4:edd43c58
    [61704.053469] [<c010ba74>] (show_stack) from [<c03c0f18>] (dump_stack+0x24/0x28)
    [61704.060747] [<c03c0ef4>] (dump_stack) from [<c012d370>] (__warn+0xe8/0x100)
    [61704.067758] [<c012d288>] (__warn) from [<c012d3c8>] (warn_slowpath_fmt+0x40/0x48)
    [61704.075297] r9:00000000 r8:ee914cd0 r7:c09b32dc r6:00000002 r5:c09b3130 r4:c09b31d4
    [61704.083099] [<c012d38c>] (warn_slowpath_fmt) from [<c03f0128>] (l3_interrupt_handler+0x25c/0x36c)
    [61704.092023] r3:ee914b00 r2:c09b31d4
    [61704.095622] r4:80080003
    [61704.098197] [<c03efecc>] (l3_interrupt_handler) from [<c016aa28>] (__handle_irq_event_percpu+0xb4/0x144)
    [61704.107742] r10:c0c179c8 r9:ee81db00 r8:00000015 r7:edd43d7c r6:00000000 r5:ee81db00
    [61704.115614] r4:ee919080
    [61704.118181] [<c016a974>] (__handle_irq_event_percpu) from [<c016aadc>] (handle_irq_event_percpu+0x24/0x60)
    [61704.127901] r10:be904ad8 r9:edd42000 r8:ee808000 r7:edd43f40 r6:00000000 r5:ee81db00
    [61704.135773] r4:ee81db00
    [61704.138339] [<c016aab8>] (handle_irq_event_percpu) from [<c016ab7c>] (handle_irq_event+0x64/0x90)
    [61704.147260] r5:c0c082a0 r4:ee81db00
    [61704.150878] [<c016ab18>] (handle_irq_event) from [<c016de28>] (handle_fasteoi_irq+0xc0/0x200)
    [61704.159452] r5:c0c082a0 r4:ee81db00
    [61704.163066] [<c016dd68>] (handle_fasteoi_irq) from [<c0169c10>] (generic_handle_irq+0x2c/0x3c)
    [61704.171735] r7:edd43f40 r6:00000000 r5:00000015 r4:c0c1f56c
    [61704.177439] [<c0169be4>] (generic_handle_irq) from [<c016a2cc>] (__handle_domain_irq+0x5c/0xb0)
    [61704.186197] [<c016a270>] (__handle_domain_irq) from [<c0101520>] (gic_handle_irq+0x40/0x6c)
    [61704.194608] r9:edd42000 r8:fa241100 r7:fa240100 r6:edd43e30 r5:fa24010c r4:c0c02c14
    [61704.202405] [<c01014e0>] (gic_handle_irq) from [<c010c58c>] (__irq_svc+0x6c/0xa8)
    [61704.209929] Exception stack(0xedd43e30 to 0xedd43e78)
    [61704.215019] 3e20: 00404100 00000100 c0c49940 00000000
    [61704.223256] 3e40: 00000202 00000012 00000000 00000000 ee808000 edd42000 be904ad8 edd43edc
    [61704.231487] 3e60: c0c49980 edd43e80 c0131048 c0130b10 600e0113 ffffffff
    [61704.238154] r9:edd42000 r8:ee808000 r7:edd43e64 r6:ffffffff r5:600e0113 r4:c0130b10
    [61704.245957] [<c0130a78>] (__do_softirq) from [<c0131048>] (irq_exit+0x140/0x144)
    [61704.253408] r10:be904ad8 r9:edd42000 r8:ee808000 r7:00000000 r6:00000000 r5:00000012
    [61704.261280] r4:c0c1f56c
    [61704.263845] [<c0130f08>] (irq_exit) from [<c016a2d0>] (__handle_domain_irq+0x60/0xb0)
    [61704.271730] [<c016a270>] (__handle_domain_irq) from [<c0101520>] (gic_handle_irq+0x40/0x6c)
    [61704.280142] r9:edd42000 r8:fa241100 r7:fa240100 r6:edd43f40 r5:fa24010c r4:c0c02c14
    [61704.287937] [<c01014e0>] (gic_handle_irq) from [<c010c58c>] (__irq_svc+0x6c/0xa8)
    [61704.295461] Exception stack(0xedd43f40 to 0xedd43f88)
    [61704.300556] 3f40: edd43fb0 00000001 00000000 600e0010 edd42000 00000000 edd43fb0 10c53c7d
    [61704.308791] 3f60: 00000000 edd42000 be904ad8 edd43fac edd43fb0 edd43f90 c0107d14 c010b3b8
    [61704.317014] 3f80: 600e0113 ffffffff
    [61704.320540] r9:edd42000 r8:00000000 r7:edd43f74 r6:ffffffff r5:600e0113 r4:c010b3b8
    [61704.328349] [<c010b368>] (do_work_pending) from [<c0107d14>] (slow_work_pending+0xc/0x20)
    [61704.336582] r7:10c53c7d r6:ffffffff r5:600e0010 r4:00010744
    [61704.342273] ---[ end trace 9394231af9932575 ]---

    Memory mapped at address 0xb6f2f000.
    Bus error (core dumped)

    Thanks,

    Nathan

  • In reply to Nathan Wright:

    Ok, this kernel panic is expected for some kernels/devices. In most of the cases pinmux register addresses are protected and cannot be accessed from user space. Sorry for misleading you on this one.

    Let me dig in further into this. I'll update as soon as I have anything.

    Best Regards,
    Yordan

     


     Please make sure you read the forum guidelines first.

  • In reply to Yordan Kovachev:

    Hello Nathan,

    TI Linux forum is going to be closed this week. In the future please use the device forum for Linux related questions on a particular device. I have moved your thread over to Sitara forum. Thank you!

    best regards,
    David Zhou

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.