This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

Linux/TMDXEVM8168: Package problem

Prodigy 170 points

Replies: 6

Views: 580

Part Number: TMDXEVM8168

Tool/software: Linux

Hello,

I am working on TMDXEVM8168 kit , when i try to install EZSDK in the supported linux (10.04 LTS) os it is showing me the error that "xinetd" package not found and even i couldn't able to install "vim or minicom" like basic packages , kindly provide me the solution and suggest me how i can compile,build and execute video and audio examples.

  • Hi Sagar,

    Do you install DM816x EZSDK 5.05.02.00? This version is supported with Ubuntu 10.04 LTS.

    software-dl.ti.com/.../index_FDS.html

    Please provide full console log of the EZSDK installation procedure, including your error message.

    Regards,
    Pavel



  • In reply to Pavel Botev:

    Hello Pavel,
  • In reply to sagar minchnal:

     Hello Pavel,

    i succesfully installed and i can able to create bootable sd card for the kit ,in which the demo can be executed using matrix GUI application,but when i tried to setup the ezsdk environment by using "./setup.sh" from installed TI_EZSDK folder as mentioned in the software developer guide i m getting "xinetd" error and if i try to install basic packages like "vim or minicom" getting error as shown in the below attached picture.

  • In reply to sagar minchnal:

    i am able to create bootable sd card for TMXDM8168 kit,how i can compile ,build and execute the sample application using Sourcery g++ lite ?kindly provide me solution for this.
  • In reply to sagar minchnal:

    sagar minchnal
    i succesfully installed and i can able to create bootable sd card for the kit ,in which the demo can be executed using matrix GUI application,but when i tried to setup the ezsdk environment by using "./setup.sh" from installed TI_EZSDK folder as mentioned in the software developer guide i m getting "xinetd" error

    Please provide the full console log of the setup.sh command execution output.

    sagar minchnal
    and if i try to install basic packages like "vim or minicom" getting error as shown in the below attached picture.

    The vim editor is not specific for the DM816x EZSDK. It is generic. I am able to install vim successful on my Ubuntu 14.04 LTS 64-bit PC. I would suggest you to ask/post in generic Linux/Ubuntu forums regarding vim editor installation issue.

    Regards,
    Pavel



  • In reply to sagar minchnal:

    sagar minchnal
    i am able to create bootable sd card for TMXDM8168 kit,how i can compile ,build and execute the sample application using Sourcery g++ lite ?kindly provide me solution for this.

    Refer to:

    ti-ezsdk_dm816x-evm_5_05_02_00/docs/DM816x_EZ_Software_Developers_Guide.pdf

    2.2 Writing your own "Hello World!" application and executing it on the target

    Regards,
    Pavel



This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.