This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

RTOS/TMDSEMU560V2STM-U: TMDSEMU560V2TM-U is broken.

Prodigy 30 points

Replies: 1

Views: 57

Part Number: TMDSEMU560V2STM-U

Tool/software: TI-RTOS

It feels like the cable connected to the CPU is out of EVM.

Error message is attachedError Message.docx.

  • Guru 140165 points
    Hi,

    Please check the explanation of the error message at the Debugging JTAG page below (search for the error number)
    software-dl.ti.com/.../ccs_debugging_jtag_connectivity_issues.html

    You are correct that there is a possibility the Debug Probe cable is broken, but more tests are required. Check if the cable is firmly secured to the main probe and, if you have an extra unit, you can try to swap the cables between the two units. Also, make sure the target board is properly powered up and running, given that sometimes the point of break can be confused by the surrounding conditions. If you have a spare target board, even better - this will be an extra helper to isolate the issue.

    If nothing actually works, then you may need to return your Debug Probe for repair or for a simple return.

    Hope this helps,
    Rafael

    When posting, click on the link Insert Code, Attach Files and more... to attach images, files or use nice formatting.

    If my reply answers your question please click on the green button "This resolved my issue".

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.